Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Where can I find the example project used in the Prof IoT article on the ITM?

Last Updated:12/27/2017

Question:

Where can I find the example project used in the Prof IoT article on the ITM?

Answer:

The example project used in the article is attached to this article. Simply import the project, follow along with the Prof IoT blog post and you will see the output described in the post.
Suitable Products
SSP
  • Was this article helpful?