Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Where can I find the lab presetations and code from the DevCon extension seminars?

Latest Updated:10/13/2016

Question:

Are the lab presentations and code available for the Devcon Extension seminars?

Answer:

You can find the lab presentations and code in the attached zip file. You need to use them as-is however since they don't have an FAE attached. 

https://knowledgebase.renesas.com/@api/deki/files/343/Archive.zip

  • Was this article helpful?