Skip to main content
Renesas Electronics Europe - Knowledgebase

Where can I find the completed telnet project for the console swap demo on the SK-S7G2 Kit?

Latest Updated:10/13/2016


Where can I find the completed Telnet version of the console swap demonstration?


The completed project, in Synergy Import format is attached below. It uses the default setting for the Ip address on the kit and was tested using a IP address on the PC Ethernet Adaptor.

  • Was this article helpful?