Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What switch settings should be set for the weather panel application project on the DK-S7G2?

Latest Updated:10/18/2016

Question:

What switch settings are needed for the weather panel application project on the DK-S7G2 kit?

Answer:

You should make the following settings to the switches on the DK-S7G2 kit for the weather panel application project: Set DRAM switch on S5 (bottom left corner of the motherboard) to On. Set CAM, MMC and SD switches on S101 (bottom left corner of the baseboard) to off.
Suitable Products
DK-S7G2