Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

I get a compile error with the messaging framework when I have C++ code. What is going on?

Last Updated: 04/08/2016

Question:

I'm getting a compile error in the messaging framework with my C++ code. What is going on?

Answer:

There is a bug in the messaging framework code. This bug comes about because the name 'class' was used in the messaging framework as a variable name and it is a C++ reserved word. This bug has been identified and is in the fix queue. When we have an estimate fix date, this article will be updated with the release date for the fix.

  • Was this article helpful?