Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

USBX Device Class HID Module Guide Resources

Last Updated:03/01/2018

Question:

Where can I find the resources for the USBX Device Class HID module guide?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The USBX™ Device Class HID module is a high-level API for human interface device (HID) applications and is implemented on g_ux_device_class_hid. The USBX Device Class HID module configures the USBX Device Class HID Source, USBX Host Configuration, USBX Source and USBX Port HCD. The USBX Device Class HID module uses the USB peripheral on the Synergy MCU.

 

Module Guide

The USBX Device Class HID module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The most recent versions of the USBX Device Class HID module guide application note, application project and import guide are available here.

Module Guide Resources

The following useful user manuals are included in the X-Ware documentation package available here.

  • USBX Host Stack User’s Manual
  • USBX Device Stack User’s Manual

The following useful module guides and application projects are available from the Renesas web site:

  • USBX Device Class HID Module Guide- Application Project here.
  • USBX Device Class Mass Storage Module Guide- Application Project here.
  • USBX Device Class CDC-ACM Module Guide- Application Project here.
  • USBX Host Class HUB Module Guide- Application Project here.
  • USBX Host Class CDC-ACM Module Guide- Application Project here.
  • USBX Host Class Mass Storage Module Guide- Application Project here.

You can find all USBX Synergy projects and documents by searching for "USBX Synergy" on Renesas.com here.

 

Known issues

  • Refer to the SSP release notes for known issues, available here.

 

Suitable Products
SSP