Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

SSP Version 1.4.0 Usage Notes

Last Updated:03/30/2018

SSP Version 1.4.0 usage notes can be found in the attached PDF.

The usage notes include issues and workarounds for BSP, HAL, Framework, and Express Logic modules, as well as MCU implementation/SW architecture.

sspv140-v101_Additional-Usage-Notes.pdf

 

  • Was this article helpful?