Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

R_ADC Module Guide Resources

Last Updated:04/25/2017

Question:

Where can I find the references to module guide resources for the ADC HAL module on r_adc?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Question:

Where can I find the references to module guide resources for the ADC HAL module on r_adc?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The ADC HAL module is an API for analog-to-digital conversions and is implemented on r_adc. It supports both the ADC12 and ADC14 peripherals available on Synergy microcontroller hardware. A user-defined callback can be created to process the data each time a new sample is complete.

The ADC HAL module supports the following features:

  • 14-Bit A/D Converter (S3A7, S124) or 12-Bit A/D Converter (S7G2)
  • Multiple Operation Modes:
  • Multiple Channels

Module Guide

The ADC HAL module guide is targeted for SSP 1.2.0 and the SK-S7G2 Kit.

The most recent versions of the ADC HAL module guide application note, application project and import guide will soon be available from the Synergy Gallery:  here

Module Guide Resources

  • Wi-Fi Application on SK-S7G2 using Wi-Fi Framework with SSP 1.2.0
  • LPM ADC DK-S124 with SSP 1.2.0
  • OOB image and source project with SSP 1.2.0
  • Simple PMOD LCD Example for DK-S124 with SSP 1.2.0
  • Simple record/playback using ADC framework for SSP 1.2.0
  • HMI Brushless DC (BLDC) Motor Controller - Application Project
  • Bluetooth Low Energy on DK-S7G2 and DK-S3A7
  • Getting Started with the Audio Player Application using SSP
  • Developer Examples

Known issues

  • No known issues as of posting date
ADC HAL module on r_adc (SSP 1.2.0)
  • Was this article helpful?