Skip to main content
Renesas Electronics Europe - Knowledgebase

NetX FTP Server Module Guide Resources

Last Updated:03/02/2018


Where can I find the references to module guide resources for the Express Logic NetX™ and NetX™ Duo FTP Server module?


Information on the module guide itself and the associated resources and known issues are available here.


The File Transfer Protocol (FTP) is a protocol designed for file transfers. FTP utilizes reliable Transmission Control Protocol (TCP) services to perform its file transfer function. Because of this, FTP is a highly reliable file transfer protocol. FTP is also high-performance. The actual FTP file transfer is performed on a dedicated FTP connection. NetX™ FTP is specific to IPv4. NetX Duo™ FTP accommodates both IPv4 and IPv6 networks. IPv6 does not directly change the FTP protocol, although some changes in the original NetX FTP API are necessary to accommodate IPv6 and will be described in this document.

The module supports the following features:

  • NetX is IPv4 specific
  • NetX Duo supports both IPv4 and IPv6 networks
  • Works with FileX® file system
  • No limit to file name size; uses NULL terminated ASCII strings
  • Supports TCP port 21 to field client requests
  • Provide high-Level APIs for creating, starting, stopping and deleting service
  • NetX FTP and NetX Duo FTP are compliant with RFC 959, RFC 2428 and related RFCs.

Module Guide

The module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The most recent versions of the module guide application note, application project and import guide are available here.

Module Guide Resources

The Express Logic User Manual for the NetX and NetX Duo FTP Server is available from the X-Ware Component Documents for Renesas Synergy zip file located at the bottom of the web page here.

Many NetX and NetX Duo related application projects are available from the Renesas web site. A few examples are listed below.

  • NetX™ Duo DHCP Client Module Guide- Application Project here.
  • NetX™ Duo FTP Client Module Guide- Application Project here.
  • NetX™ Duo NAT Module Guide- Application Project here.
  • NetX™ and NetX™ Duo Auto IP Module Guide- Application Project here.

To find ALL available NetX related module guides, simply search for "NetX Module Guide Synergy" on the Renesas web site search bar, and specify Application Notes in the document type Search Results filter, like this.

You can similarly search for Net Duo related module guides, like this.

Known issues

  • Refer to the SSP release notes for known issues, available here.
Suitable Products