Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Module Guide Test- r_adc HAL Module

This guide provides details on using the r_adc HAL Module in a Synergy Platform project.

You can find an Introduction to the module, detailed definitions for each API function, an Operational Overview including limitations and design considerations, steps for Adding the module to a project and Configuring it, a description of the programming steps used in a typical application and a walk through of the associated Application Project code.

  • Was this article helpful?