Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

r_doc Module Guide Resources

Latest Updated:4/18/2017

Question:

What resources are available for the r_doc module?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Module Guide

The r_doc HAL module guide is targeted for SSP 1.2.0 and the SK-S7G2 Kit.

The r_doc HAL module guide describes what the module does, how to add it to your project, how to configure it, the associated APIs and provides an application project with a code walk through so you can quickly learn how to use the r_doc HAL module in your own design. We recommend that you have the SSP ISDE open and inspect the module stack, configuration information and code while reading over the application project description.

The most recent versions of the r_doc HAL module guide application note, application project and import guide are available here

Know issues

  • Refer to the most recent release notes for known issues, available here.

Associated Resources

  • None available currently