Skip to main content
Renesas Electronics Europe - Knowledgebase

How do Install the USB Driver for the SSP e2 studio debug connection to a Synergy kit?

Latest Updated:10/04/2016


How do I install the debug interface USB driver for e2 studio and SSP to communicate to my Synergy Kit?


The driver should be installed automatically when you install e2 studio and SSP. It will show up as the J-Link driver in the USB section of Windows Device manager.



If for some reason it doesn't show up, you can install the driver manually from the Segger web site here: