Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How do I manually assign the SEGGER CDC UART driver to the "EL Composite Device" in Windows?

Latest Updated:10/04/2016

Question:

How do I manually assign the SEGGER CDC UART to the EL Composite Device?.

Answer:

If you installed the J-Link package (available here: https://www.segger.com/jlink-software.html), you can manually assign SEGGER CDC UART driver to the "EL Composite Device". Attached, find a short clip showing you how to do that. You'll need sufficient privileges to open Device Manager (Win+R >> "devmgmt.msc"). the answer.