Skip to main content
Renesas Electronics Europe - Knowledgebase

How do I implement screen rotation on the framework level in SSP?

Latest Updated:10/02/2016


I want to rotate my screen by 90 degrees on my Synergy Kit within SSP. Is there an easy way to do this?.


A rotation feature, at the Framework Level, will be implemented in SSP release 1.1.0 so it will be very easy to do this after that release, currently scheduled for around the end on May 2016. Once available a simple example will be posted to this article.