Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How do I create a Custom Board Support Package for an SSP Project?

Latest Updated:09/09/2016

Question:

How do I create a custom board support package when using the Synergy Software Package?

Answer:

You can create a custom board support package (BSP) using a special tool- the BSP Custom Creator Tool. A custom BSP is usually required when you create your own target board.

 

The tool has 4 steps and uses 2 executable functions.

1) Create a base BSP from and existing BSP (Custom BSP Creator)

2) Create template pack using base BSP (Custom Pack Creator)

3) Modify BSP for custom board (User work)

4) Create final pack for custom board (Custom Pack Creator)

 

These steps and the detailed process for using them can be found in the associated application note: