Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How do I change the Ethernet reset pin to work on the SK-S7G2 kit?

Latest Updated:09/19/2016

Question:

The Ethernet reset pin is incorrect for the SK-S7G2 kit. How do I change it to operate correctly?

Answer:

The Ethernet reset pin is incorrectly assigned to P7_06, the pin used on the DK kit.
When the SK is selected the pin remains unchanged, so it must be changed manually to the correct location of P8_06. Change this field in the  Ethernet properties window as shown below (change the P7_06 pin to P8_06).

EnetReset.png