Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How do I Calibrate the Temperature Readings for the Synergy TSn?

Last Updated: 03/04/2016

Question:

How do I calibrate the TSn so I can get the same readings from chip to chip?

 

Answer:

In the initial Synergy MCU silicon, WS2, the TSn readings are not calibrated, so you may find variations from chip to chip. In production devices the calibration registers will be set correctly.