Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Can I set my license file for the entire workspace instead of on a project basis?

Latest Updated:09/18/2016

Question:

Can I set my license file for my workspace instead of on a project basis?

Answer:

In the SSP 1.1.0 release when you set a License File it applies to the entire workspace- so you don't need to set it every time you import a project. You can set the License File by selecting Window>>Preferences.

LicenseSet.png

Then select C/C++>>Renesas>>License.

LicenseFileSEt.png

When importing a project from 1.0.0 or earlier, you'll need to go to Project Properties>> C/C++ Build>> Environment and if AMS_LICENSE_PATH is highlighted in yellow (i.e. setting comes from USER:CONFIG), then you should select it and click Delete:

LicensePath.png  
Suitable Products
Synergy
  • Was this article helpful?