Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Can I Easily Swap my Console Framework from USB to Ethernet?

Latest Updated:10/2/2016

Question:

Can I easily swap my console framework from a USB connection to an Ethernet connection?

Answer:

You will be amazed at how easily you can swap a console framework based USB implementation to an Ethernet one. Because the Console Framework is connection independent (it doesn't care where the commands come from or the results go). You can simply remove the USB related configuration settings and swap in Ethernet Telnet configuration components. You set a couple parameters like the channel and interrupt priority and you are good to go! No code required! The attached quick start guide and the associated project file can be used to try this out using simple console demonstration.

 ConsoleSwapQSG021192016.pdf

ConsoleSwapUSB.zip

If you want to try and create the project from scratch, the code you need is attached in a .txt file. (This is an optional extra credit assignment only!)

Swap.txt
Suitable Products
SSP Console Framework