Skip to main content
Renesas Electronics Europe - Knowledgebase

Which tools matched using uPD780022 as a substitute for uPD78P014?

Latest Updated:12/01/2011


Which development tools are compatible when using the uPD780022 as a substitute for the uPD78P014?


Regarding the software, the compiler or assembler can be used as is.
Please download the device file from "Download Development Tools."
Regarding the emulator, it is necessary to purchase the emulation board for the uPD78002x and a compatible probe.

Moreover, you are using the PROM version, but in the case of the uPD780022, you need to use the flash version (uPD78F0034), and the dedicated FlashPro4 as the programmer.

For more information about the required tools, refer to the device user's manual appendix.
Suitable Products
  • Was this article helpful?