Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Where can I get sockets for the H8/300H Tiny Series ?

Latest Updated:03/18/2009

Question:

Where can I get sockets for the H8/300H Tiny Series ?

Answer:

Sockets for the H8/3664F and other tiny series devices are available from the following sources. Package Socket Manufacturer DP-42S DIP642B11S1-007, ITT Cannon. FP-64A IC149-064-008-B5, Yamaichi. FP-64E IC149-064-175-B5, Yamaichi Contact details: YamaichiWorld-widewww.yamaichi.co.jp or Europewww.yamaichi.de
Suitable Products
H8/300H Tiny