Skip to main content
Renesas Electronics Europe - Knowledgebase

What should I change when "Warning: address is too long" is output

Latest Updated:12/01/2011


A compiler message "Warning: address is too long" is output after pm1.cmd.
What should I change to prevent this message from being output?


This message is output when the address range supported by the object format is exceeded in the HEX converter.
For addresses in your program, you have to use a format that supports 32-bit addresses.
Specify -fs as a HEX converter option.
For details, refer to Chapter 8 "Hexadecimal Converter" in the Operation manual.
Suitable Products