Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Where can I find the specification of the target cable of PG-FP5?

Latest Updated:11/21/2014

Question:

Where can I find the specification of the target cable provided with flash programmer PG-FP5?

Answer:

The cables for connection to the target have 14 or 16 pins.
For details of the specification, refer to the PG-FP5 Flash Memory Programmer User's Manual from here.
Suitable Products
PG-FP5