Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What to do with the error, E3204: Memory area/space 'xxx' not defined

Latest Updated:12/01/2014

Question:

I am using the CA78K0R compiler for RL78 and 78K0R products or the CA78K0 for 78K0 products, and the following error message appears when I build a project. What, if anything, should I do about it?
E3204: Memory area/space 'xxx' not defined

Answer:

The above error is output when memory area xxx specified by MERGE in the link directive file does not exist.

Memory areas may have incorrect definitions or not be specified by MEMORY in the link directive file. Check whether the area is specified by MEMORY in the link directive file and if it is, whether the specification is correct.

Suitable Products
C Compiler Package for RL78 and 78K Families
Compiler for RL78 Family and 78K0R [CA78K0R]
Assembler Package for 78K0R [RA78K0R]
Compiler for 78K0 [CA78K0]
Compiler for 78K0 [CC78K0]
Assembler Package for 78K0 [RA78K0]