Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What are the "mask option" set in the MM?

Latest Updated:09/15/2006

Question:

What are the "mask option" set in the MM?

Answer:

"Mask option", indicates special functions that can be set when creating the ROM mask. These functions are not necessary for all types of MCUs. Please refer to the Mask ROM Confirmation Form corresponding to the MCU you are using for more information concerning the mask option.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering