Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

List of FAQs for the each RL78 Self Programming Library

Last Updated:09/20/2017

Question:

List of FAQs for the each RL78 Self Programming Library

Answer:

FAQs for the each RL78 Self Programming Library are listed below.

Target Self Programming Libraries Content FAQ No.
All Libraries
List of supported devices for each library
Self-RAM area requirements for each library
Error RAM parity error
Voltage mode Setting of voltage mode
Voltage mode Difference by voltage mode
Setting of Operating frequency
Debugging by using CS+
Restrictions on using the [Link Options] tabbed page of CS+ to control the allocation of self-RAM areas
Using the short direct addressing area
Initialization of self-RAM area
Data value after erasure
Overwriting of data
Flash Self Programming Library Type01
Error Erasure error
Error Function executing error before presetting
Boot swapping Data values of the new and old boot programs after interruption of power while boot swapping
Boot swapping Boot program area after interruption of power while boot swapping
Boot swapping Value of the boot flag after interruption of power while the setting of the boot flag is being changed
Boot swapping Block numbers after boot swapping
Boot swapping Boot area in case of flash memory erasing after boot swapping
About the internal verification
Flash Self Programming Library execution Warnings W0071 and W0072 by CS+
Flash Self Programming Library execution Processing to call a function from boot area to flash area
Reading during operations of the code flash memory
If power is momentarily shut down while data in flash memory are being written or erased, what happens to the data?
Data Flash Library Type04
Rewriting and erasing data flash memory 3000158
Error Erasure error
Error Execution of the PFDL_Open() function makes program runaway.
Error Recommended methods to deal with errors: Erasure error,Blank check error ,Writing error,Internal verification error
Size of the library
Data buffer capacity
About the internal verification
Writing or erasing data without using the Data Flash Library
Reading the data without using Data Flash Library
Reading during operations of the data flash memory
If power is momentarily shut down while data in flash memory are being written or erased, what happens to the data?
EEPROM Emulation Library Pack01
When would I use EEPROM Emulation Library? What are the differences between Pack01 and Pack02?
Error An error is occurred during execution of the EEL_Init() function.
Error FAL_ERR_CONFIGURATION(0x21) error is occurred during execution of the FAL_Init function.
Recommended interval for executing the EEL_Handler function
Confirming the voltage level of writing data
Operation timing of DFLEN
Reading during operations of the data flash memory
Reading write data specified by address
Under what conditions does the status of the block status flag turn into the use prohibited?
What happens to the data and the block if power is momentary shut down during the EEL_CMD_CLEANUP command execution?
EEPROM Emulation Library Pack02
When would I use EEPROM Emulation Library? What are the differences between Pack01 and Pack02?
Error An error is occurred during execution of the EEL_Init() function.
About the internal verification
Recommended interval for executing the EEL_Handler function
Interruption of power is occurred during execution of EEL_CMD_WRITE command.
An abnormal state is occurred while an EEL_Execute function with EEL_CMD_REFRESH command was copying data to a block
Reading during operations of the data flash memory
Reading write data specified by address
Suitable Products
Flash Self Programming Libraries
Data Flash Libraries