Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is writing/erasing data in RL78 item memory possible without command?

Last Updated:04/11/2018

Question:

Is it possible to write or erase data in the data flash memory of a RL78 family without using the write or erase commands for the PFDL_Execute function of Data Flash Library Type04 for the RL78 family?

Answer:

Yes.
You can write and erase data in data flash memory by using a flash programming tool.

For information on the flash programming tools from Renesas, refer to the following Link.

Renesas Flash Programmer

 

Suitable Products
Data Flash Libraries
Renesas Flash Programmer