Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is the self RAM used in the RL78 family libraries need to be initialized?

Latest Updated:12/05/2014

Question:

Do the self RAM areas used in the following libraries for the RL78 family need to be initialized?

  • Flash Self Programming Library Type01
  • Data Flash Library Type04
  • EEPROM Emulation Library Pack01
  • EEPROM Emulation Library Pack02

Answer:

The self RAM area used in the library need not be initialized in the user program because the RAM is initialized by the initialization function of the library*.
However, if the user program uses the self RAM area for the library, make sure that the user program initializes that area.

*Note: If you are using v2.20 or an earlier version of Flash Self Programming Library Type01 and more than 1 Kbyte of self RAM is required, the user program will need to initialize the 10-byte range of addresses beyond the first Kbyte because the library does not.

Suitable Products
Flash Self Programming Libraries
Data Flash Libraries