Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is it possible to read data from other address if FSPL is running?

Latest Updated:12/12/2014

Question:

Is it possible to read data from other addresses in code flash memory possible while the Flash Self Programming Library to erase or program the code flash memory of an RL78-family product?

Answer:

Code flash memory cannot be read while operations of the flash library on the code flash memory are in progress.
Suitable Products
Flash Self Programming Libraries