Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is it OK that file codes created with different version MMs differ?

Latest Updated:09/15/2006

Question:

Is it OK that file codes created with different version MMs differ?

Answer:

Since Ver. 2.00.00, MM stores version information on the running MM in the mask file.
For this reason, the file code for mask files created with different version MMs will differ even if the same data is registered.
However, this version information has absolutely no effect whatsoever on the data to be masked, so there is no need to worry.
Also, ROM mask processing is performed correctly no matter version was used to create the mask file.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering