Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is a hexadecimal data file require an offset when working with an EPROM?

Latest Updated:09/15/2006

Question:

Does a hexadecimal data file require an offset as when working with an EPROM?

Answer:

Hexadecimal data files processed with MM use the real address of the microcomputer to be masked.
When masking with older EPROMs, it was necessary to assign an offset to the address in accordance with the EPROM product.
This is not necessary with MM.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering