Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How to properly set up invoking HEW from IO Wizard?

Latest Updated:09/04/2009

Question:

I have followed the instructions in the User Manual regarding the setup for invoking HEW from IO Wizard. However, I am still getting error message.

Answer:

IO Wizard needs to be closed and reopened if you have made any changes to the environment settings. If you are using this new function for the first time, restarting IO Wizard will solve the problem.
Suitable Products
  • Was this article helpful?