Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How to find my target MCU type code in MCU list for H8/SLP series?

Latest Updated:09/04/2009

Question:

For H8/SLP series, I could not find my target MCU type code in the MCU list ?

Answer:

On IO Wizard, the peripheral settings display for H8/38347 group is designed based on product number. Corresponding to the peripheral settings supported on IO Wizard, only product number for MCU devices is listed for user selection.

For H8/SLP series :

  1. H8/38347 group - Available product numbers are H8/38342, H8/38343, H8/38344, H8/38345, H8/38346 and H8/38347.
  2. H8/38347 group - Each product number has options for Mask ROM versions, F-ZTAT versions, Type Code, Mark Code and Package(Package Code).
Suitable Products