Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How to allocate initial values to data flash area in CA78K0R compiler?

Latest Updated:11/21/2014

Question:

I am using the CA78K0R compiler for RL78 and 78K0R products. Please show me how to allocate initial values to the data flash area.

Answer:

Allocating constant initial values requires either of the following definitions.

  • In the source file, define values by specifying addresses within flash memory for const constants.
  • In the link directive file, add a definition for the data flash area.

Example of a definition in a C-source file:

#pragma section @@CNSTL DFL_C AT 0F1000H
__far const unsigned char dfl_data_c[]={0x11,0x22,0x33,0x44}; 
#pragma section @@CNSTL @@CNSTL

Example of a definition in the link directive file:
MEMORY DATFL : (0F1000H,1000H)
Suitable Products
C Compiler Package for RL78 and 78K Families
Compiler for RL78 Family and 78K0R [CA78K0R]