Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Generating code at switching the build mode

Last Updated:05/24/2017

Question:

Should I perform “Generate Code” in each mode at every time when switching the build mode (Ex. Debug, Release, etc.)?

Answer:

We recommend you to do so since the compile options for option byte and on-chip debugging operate with the code generator.

The settings of option byte and on-chip debugging reflect values set by the code generator.

If you change the settings of the high-speed on-chip oscillator, LVD, or the watch dog timer, it affects the option byte. Therefore, if you change the settings of these functions, perform “Generate Code” in each build mode.

 

Suitable Products
Code Generator