Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Does the compiler secure the required stack size?

Latest Updated:12/01/2011

Question:

The CC78K0 expanded functions include interrupt functions.
If stack switching specification has not been used, does the compiler secure the required stack size?

Answer:

No, CC78K0 does not secure stack area separatly, and only uses default stack area.
Suitable Products