Skip to main content
Renesas Electronics Europe - Knowledgebase

Data Reading Addresses: DFL Type04 EEPROMEL Pack01 EEPROMEL Pack02

Latest Updated:12/12/2014


Is it possible to read data from other addresses in data flash memory while using one of the following libraries to erase or program the data flash memory of an RL78-family product?

  • Data Flash Library Type04
  • EEPROM Emulation Library Pack01
  • EEPROM Emulation Library Pack02


Data flash memory cannot be read while operations of the flash library on the data flash memory are in progress.
Suitable Products
Data Flash Libraries