Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Can RTOS : pSOS or ╬╝ITRON be mounted on the V850 ?

Latest Updated:12/01/2011

Question:

Can RTOS : pSOS or μITRON be mounted on the V850 ?

Answer:

Our product RX850 conforms to μITRON3.
In addition, regarding pSOS, a product that supports the V850E is available from a third-party company.

Contact the following company for details:

Integrated Systems Japan
TEL 03-3492-3171
FAX 03-3492-3066
E-mail info@isi.co.jp
HP http://www.isi.com/
Suitable Products