Skip to main content
Renesas Electronics Europe - Knowledgebase

Can "H8SX family" be developed with compilers (PS008CAS5-MWR etc.)?

Latest Updated:09/10/2007


Can an "H8SX family" be developed with the compilers (PS008CAS5-MWR etc.) that are not compliant with the "H8SX family"?


The object programs for H8S can be executed in H8SX.
A program for H8SX can be developed using the development environment for H8S (Compiler and assembler), but new functions of H8SXCPU are not available.
Suitable Products
C/C++ Compiler Package for H8SX, H8S, H8 Family