Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Bus width cannot be set to 16-bit or 32-bit in RX Code Generator Plug-in

Last Updated:08/02/2017

Question:

How can I set bus width to 16-bit or 32-bit in the RX Code Generator Plug-in or AP4 for RX?

Answer:

To specify 16-bit or 32-bit bus width, select the BC1/WR1 pin check box. For details, refer to "16.4.1 Data Alignment Control for CS Area" in the user's manual for hardware.

3000137.PNG

Example: When selecting the CS1 bus width in RX71M buses

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
Code Generator