Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What happens when FPU attribute is specified for a task without floating point calculation

Last Updated:03/22/2017

Question:

Is it OK to specify FPU attribute TA_COP1 for a task that does not perform floating point calculation?

Answer:

Yes, it is OK. However, note that it may consume more stack memory and take more time for dispatching, compared to when TA_COP1 is not specified
Suitable Products
HI7000/4
  • Was this article helpful?