Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Setting of Real-time OS base clock in sample project using FIT

Last Updated:06/28/2017

Question:

Which value should I set as the RTOS base clock in the RI600V4/RI600PX sample project using FIT?

Answer:

For the base clock (clock.timer_clock in the sample.cfg file), set the clock frequency for PCLKB that is set in r_bsp_config.h.
This makes the period of the base clock approximately 1 ms.

Setting examples:

 For RX71M_RI600V4_FIT or RX71M_RI600PX_FIT, clock.timer_clock = 60 MHz

 For RX64M_RI600V4_FIT or RX64M_RI600PX_FIT, clock.timer_clock = 60 MHz

 For RX63N_RI600V4_FIT or RX63N_RI600PX_FIT, clock.timer_clock = 48 MHz

 For RX210_RI600V4_FIT, clock.timer_clock = 25 MHz

 For RX113_RI600V4_FIT, clock.timer_clock = 24 MHz

Suitable Products

RI600V4
RI600PX
RX Family