Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Interrupt handler is being called repeatedly

Last Updated:03/22/2017

Question:

An interrupt handler is being called repeatedly.

Answer:

The interrupt handler may be called repeatedly until the interrupt factor is cleared.
Suitable Products
HI7000/4