Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What do this error "Can't find flash memory tool file" mean?

Latest Updated:03/31/2009

Question:

When I download my program, the following message is displayed on the screen:
"Can't find flash memory tool file"

Answer:

If you are only downloading the program to the RAM area, you need to disable Loading Flash Memory on the Loading Flash Memory page in the Configuration dialog box.
If you are downloading to the external Flash ROM, this message might have been generated because you are using an older version of emulator software. In this case, please update to the latest version of your emulator software.
Suitable Products
E10A-USB
R0E0200F0EMU00
R0E0200F1EMU00
R0E0200F2EMU00