Skip to main content
Renesas Electronics Europe - Knowledgebase

There's a black spot on surface of E1/E20 emulator's case. What is it?

Latest Updated:03/21/2013


There is a tiny black spot on the surface of the E1/E20 emulator's case. What is it?


It derives from an environmentally-friendly, vegetable-based material used for the casing. The E1/E20 emulator's casing material is based on polylactic acid, or polylactide.
Please note that the tiny spot is not a defect in the product.
Suitable Products
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]