Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How to install emulator with E10A-USB to E10A-USB to add other device?

Latest Updated:09/10/2007

Question:

Can I install an emulator software license bundled with E10A-USB product package to the other E10A-USB emulator to add another device group?

Answer:

No, You cannot. The emulator software licensebundled with E10A-USB product package can be used one time only to install one device group when the E10A-USB emulator is unused (in initial condition). Therefore, the license cannot be used for E10A-USB emulator which the other device group previously installed.
Suitable Products
E10A-USB