Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Error Message-Memory area error. It is outside the effective address range_E8a_E8

Last Updated:10/11/2017

Question:

When downloading a load module connecting the E8a/E8 to a target board, the error message "Memory area error. It is outside the effective address range" is displayed.

Answer:

When downloading a load module connecting the E8a/E8 to a target board, the error message "Memory area error. It is outside the effective address range" is displayed.

Suitable Products

E8a
E8
  • Was this article helpful?