Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

E1 Self-Checking Error_Error 2230

Last Updated:02/21/2018

Question:

Error 2230 occurred during self-checking of the E1 emulator.
Is the E1 emulator damaged?

Answer:

Error 2230 is a common error that indicates damage in the E1 emulator.
The error is related to the user interface, and indicates that the E1 emulator or user interface cable might be damaged. 
For repair, contact your local distriburor.

Suitable Products

E1 Emulator