Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Can E8a be used to debug H8S, H8SX or SH MCUs?

Latest Updated:06/27/2011

Question:

Can E8a be used to debug H8S, H8SX or SH MCUs?

Answer:

E8a only supports the H8S/Tiny series of the H8S family.

E8a cannot be used to debug any other series’ in the H8S, H8SX or SH families. Some types of H8S, H8SX or SH family MCUs can be debugged using the E10A-USB on-chip emulator.
Always confirm the E10A-USB emulator Target devices before use.
Suitable Products
E8a