Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

"E10A-USB software doesn't normally start; HEW terminates WRONGLY. "

Latest Updated:10/04/2012

Question:

In the PC which uses a device that virtually assigns the USB port to TCP/IP, the E10A-USB emulator software is not initiated normally, and the High-performance Embedded Workshop terminates abnormally.

Answer:

There is a possibility that the utility software for the device which virtually assigns the USB port to TCP/IP is conflicting with the E10A-USB emulator software. After uninstalling the utility software for the device which virtually assigns the USB port to TCP/IP, confirm the operation of the E10A-USB.

If the E10A-USB operates normally, use the E10A-USB in that state.

Suitable Products
E10A-USB